NEWS
Product News and Information from Greenheck
CORPORATE INFORMATION
Greenheck Group, the world’s leading manufacturer of air movement, control, and conditioning equipment with manufacturing locations across the United States, was named as one of Forbes’ America’s Best Midsized Employers on...
Retrofit magazine recently recognized Greenheck model ECV-40 as one of the publication’s Top 25 Products of 2020. The eighth annual Top 25 Products, which appears in Retrofit’s January/February 2021 issue, celebrates the products that received...
December, 2020 - Greenheck Group to Acquire Metal Industries
The Greenheck Group announced today that it has signed a letter of intent to acquire Metal Industries, a leading manufacturer of grilles, registers, diffusers, and air terminal products used in commercial and institutional buildings. The addition...
December, 2020 - Greenheck HVLS Fan Wins Consulting-Specifying Engineer 2020 Product of the Year Award
Greenheck model DC-5, high volume low speed (HVLS) fan, received the gold level recognition as a Consulting-Specifying Engineer (CSE) 2020 Product of the Year. The award, voted on by the publication’s readers, was selected as the top product of the year in...
September, 2020 - Bernard A. Greenheck Education Center Doesn't Stop for Pandemics
In a typical year, Greenheck hosts hundreds of people from around the world at its Schofield, Wisconsin campus for the company’s extensive HVAC University training programs. In 2020, COVID-19 quickly put a temporary halt to that. However, not even a pandemic could prevent Greenheck from...
September, 2020 - Greenheck Opens New Louver Plant in Shelby, NC
Greenheck recently expanded its louver manufacturing capacity with a new 120,000-square-foot facility at its Shelby, North Carolina campus. The expansion significantly increases Greenheck's overall louver manufacturing footprint and supports the company's focus on...
August, 2020 - Model DC-5 HVLS Fan Receives Engineered Systems’ 2020 Commercial Comfort Product of the Year
Model DC-5 high volume low speed (HVLS) fan has won Engineered Systems’ 2020 Commercial Comfort Product of the Year Award in the IAQ/Ventilation category. Winners were officially announced in the...
July, 2020 - Product of the Year Voting Underway
Consulting Specifying Engineer (CSE) has named the Greenheck model DC-5 as a finalist for its Product of the Year award, in the HVAC category. The publication uses the award to highlight new products in the HVAC, fire/life safety...
March, 2020 - Greenheck Group Producing Essential Air Movement Equipment to Support Healthcare During COVID-19 Pandemic
As multiple state and government agencies have limited travel and ordered people to shelter in their place of residence, essential businesses like Greenheck
Group are addressing new challenges...
Retrofit magazine recently recognized Greenheck model DS high volume low speed (HVLS) fan as one of the publication’s Top 50 Products of 2019.
February, 2020 - Greenheck Group Receives Wisconsin Manufacturer of the Year Award
Greenheck Group, one of the world’s leading manufacturers of air movement, control and conditioning equipment with corporate headquarters and several manufacturing facilities in Schofield, Wisconsin, was selected as the 2019 Wisconsin Manufacturer of the Year...
FANS
January, 2021 - New Mixed Flow Square Inline Fans from Greenheck
Greenheck direct drive square inline fans now incorporate mixed flow wheel technology for a unique combination of high efficiency, low sound and ease of installation in a square housing design. AMCA certified for sound and air performance, mixed flow model SQ is...
October, 2020 - Greenheck Introduces Three-Phase Vari-Green® Motors
Greenheck has added three-phase motors to its line of energy efficient Vari-Green® electronically commutated (EC) motors. The new three-phase motors accept 208-230V and 460V power supply and are available in sizes ranging from...
August, 2020 - Greenheck Offers More Ceiling Radiation Damper/Bath Fan Combinations for Wood Truss Applications
Greenheck’s new ceiling radiation damper model CRD-320WT, combined with select models of Greenheck ceiling exhaust bathroom fans, adds even more code-compliant options for wood truss applications. The CRD-320WT damper is UL approved for...
June, 2020 - Greenheck Introduces Five-Blade Commercial HVLS Fan
Greenheck’s line of high-volume low-speed (HVLS) fans continues to grow with the addition of model DC-5, a five-blade HVLS fan incorporating a sleek, lightweight design. DC-5 fans weigh less than 100 pounds and feature...
Greenheck’s model GJI is the latest in its GreenJet® series of fans specifically designed to ventilate enclosed parking structures. Featuring a low profile of less than 12 inches, the GJI ductless jet fan maximizes...
LABORATORY EXHAUST SYSTEMS
Greenheck’s Vektor®-H laboratory exhaust fans are now available with a reduced maintenance direct drive fan design for high efficiency operation, lower sound levels, and reduced long-term operating costs. The Vektor-H is a...
Greenheck’s Vektor-H® high plume laboratory exhaust systems in single and two fan configurations can now be specified with a factory-preprogrammed controls package. The independent control system maintains duct static pressure by modulating fan speed, bypass damper position, and isolation dampers...
DAMPERS
November, 2020 - New Round Industrial Control Damper From Greenheck
Greenheck has introduced a round industrial control damper to accommodate higher velocities and pressure. Model HCDR-450 is rated for velocities up to 7000 fpm and pressure up to 30 in. wg, and withstands temperatures from...
September, 2020 - Greenheck Redesigns AMD Line of Air Measuring Dampers
Greenheck recently redesigned its AMD line of Air Measuring Dampers that combine an accurate airflow measuring station and a low leakage control damper into one compact unit. The differential pressure Air Measuring Station (AMS) now includes...
Greenheck has introduced two new heavy-duty industrial control dampers for high temperature applications. Models HCD-324 and HCD-524 feature a high temperature blade design to control...
July, 2020 - Greenheck Introduces Outdoor Electric Duct Heater
Greenheck’s latest electric duct heater, model IDHE-O with a NEMA 4 enclosure, is UL listed for outdoor applications. The IDHE-O allows for multiple mounting positions where the control cabinet can be installed...
Model ABD-Z1 is the latest addition to Greenheck’s line of automatic balancing dampers that provide on-demand control to ventilation systems. Model ABD-Z1 combines a shut-off damper with an electric actuator, automatic balancing damper (ABD) and ...
LOUVERS
December, 2020 - Greenheck Introduces High-Performance Drainable Louver
Greenheck’s ESD-635HP, a 6-inch deep stationary drainable blade louver, is designed to provide high volume air flow and superior resistance to water penetration. The high-performance ESD-635HP incorporates drain gutters in the head member and...
DEDICATED OUTDOOR AIR SYSTEMS (DOAS)
January, 2021 - Greenheck Expands Dedicated Outdoor Air Systems Line
Greenheck’s line of Dedicated Outdoor Air Systems (DOAS) for high percentage and 100% outside air continues to grow with the addition of two new models. Pre-engineered rooftop ventilator models RV-75 and RVE-150 with energy recovery offer...
An air-source heat pump option is now available on Greenheck model RV and RVE dedicated outdoor air systems. Air-source heat pumps are refrigeration systems that provide...
MAKE-UP AIR
Greenheck make-up air models DGX and MSX can now be configured with a direct drive, mixed flow plenum supply fan for...
ENERGY RECOVERY VENTILATORS
Model ECV-40 is the latest addition to Greenheck’s energy core ventilator (ECV) line. The ECV-40’s new design features a dual-fan arrangement consisting of direct drive mixed-flow plenum fans with...
October, 2019 - Greenheck’s Energy Core Ventilator Line Continues to Grow
Energy Core Ventilators (ECV) from Greenheck transfer both sensible (heat) and latent (moisture) energy between the exhaust and supply airstreams without the airstreams mixing. The energy recovery core separates ...